Skip to content

Hardware Setup ​

This guide covers the physical setup steps required before operating AI Worker, including power-on, port identification, and Remote E-STOP usage.

INFO

  • The term Follower refers to the body of the AI WORKER robot.
  • Make sure to check which robot model you are using before following the steps below.

Power On and Check Ports ​

Powering On the FFW_BG2 Follower ​

Back of the BG2 Base

  1. Toggle the Power Supply Switch to the right.
  2. Insert the Key Switch and turn it to the 12 o'clock position.
  3. Press and hold the Power Button for 3 seconds. When you hear a beep, the system is powered on. You should see the robot's head light up at this point.

Hardware Ports (FFW_BG2 Follower) ​

Back of the BG2 Body The back of the Follower body includes several ports for system access and external connections:

  • LAN Port: Used to access the robot PC via SSH or remote desktop.
  • USB Ports: For connecting peripherals such as a keyboard, mouse, or USB drive.
  • HDMI Port: Allows direct video output for connecting a monitor.

Remote E-STOP Usage ​

remote_e_stop

The Remote E-STOP device is the safety stop controller for AI Worker. It is used to perform an emergency stop and to release the initial safety lock.

Press the red mushroom button circled above to activate the E-STOP.

To release it, rotate the button clockwise, then press the A button.

The other buttons have no function.

WARNING

When AI WORKER is powered on for the first time, it remains in a torque-off state. To enable communication with the DYNAMIXELs, you must press the A button on the Remote E-STOP. When the safety lock is released, you will hear a beep sound.

Optional: ROBOTIS Hand Installation ​

If your application requires a multi-functional grip, you can replace the RH-P12-RN gripper with a ROBOTIS Hand. Follow these steps to perform the exchange:

  1. Remove the RH-P12-RN Gripper: Carefully unscrew the mounting bolts and disconnect the communication cable from the current gripper.

hand_mount_bracket

  1. Reorient the Mounting Bracket: Unscrew the mounting bolts on the FRP42-A110K bracket and rotate it by 90°. Align the bracket and mount the bolts into the highlighted holes as shown in the image above.
  1. Connect the Communication Cable: Plug the 4-pin JST cable into the port located on the ROBOTIS Hand. Ensure the connector is fully seated to prevent signal loss or intermittent connectivity.

  2. Secure the ROBOTIS Hand: Align the hand with the rotated FRP42-A110K bracket and tighten the mounting screws.

The hardware installation is now complete.

AI Worker and AI Manipulator released under the Apache-2.0 license.