Skip to content

Software Setup ​

This guide explains how to connect to the robot PC and prepare a development environment for AI Worker on a separate user PC.

INFO

The robot PC inside AI Worker is already pre-configured. Follow this guide when you want to access the robot remotely or set up a development environment on your own machine.

Accessing the Robot PC via SSH ​

AI Worker supports mDNS, allowing you to connect without manually checking the IP address.

  1. Connect the SBC (robot PC) to the same network as your user PC using a LAN cable.

  2. On your user PC terminal, run:

    bash
    ssh robotis@ffw-SNPR48A0000.local

Replace SNPR48A0000 with the serial number printed on the back of the robot body. Back of the Follower 3. When prompted, enter the system password root.

If hostname-based access is not available, use one of the following methods:

  1. Connect both your user PC and the AI Worker LAN port to the same router using Ethernet cables, then try SSH again.
  2. Connect a monitor to the Orin via HDMI, log in locally, and check the current IP address before connecting through SSH.

Development Environment Overview ​

AI Worker relies on two main repositories:

  • ai_worker: Provides support for controlling DYNAMIXEL actuators using ros2_control and enables teleoperation functionality.
  • physical_ai_tools: Provides tools for data collection, training, model inference, and visualization.

DANGER

⚠️ On the AI Worker Orin: Do not run apt upgrade. Upgrading system packages may create conflicts and break robot functionality.

Prerequisites ​

  • Operating System: Ubuntu environment
    • The AI WORKER software runs inside a Docker container based on Ubuntu 24.04 (ROS 2 Jazzy), so the host Ubuntu version on the user PC does not need to match exactly.
  • Container Engine: Docker Engine
  • Version Control: Git
  • Graphics Support
    • NVIDIA Graphics Driver
      • (In Docker-based environments, the container is generally isolated from the host system. However, the graphics driver version on the host can have a direct impact on performance and compatibility—especially when using GPU acceleration. We recommend using the following driver version(s) for best results)
      • Install nvidia-driver-570-server-open for CUDA 12.8
      • Verify the driver with nvidia-smi
    • NVIDIA Container Toolkit

Configuration ​

Docker Volume Management ​

The Docker container uses the following volume mappings for data persistence and hardware access:

yaml
volumes:
  # Hardware and System Access
  - /dev:/dev
  - /tmp/.X11-unix:/tmp/.X11-unix:rw
  - /tmp/.docker.xauth:/tmp/.docker.xauth:rw

  # Development and Data Storage
  - ./workspace:/workspace
  - ../:/root/ros2_ws/src/ai_worker/
  - ./lerobot/outputs:/root/ros2_ws/src/physical_ai_tools/lerobot/outputs
  - ./huggingface:/root/.cache/huggingface

WARNING

Container data is volatile and will be lost when the container is removed. Store important files in mapped volumes such as /workspace, the mapped source directory, model output directories, and the Hugging Face cache.

Container Management ​

  1. Clone the repository:

    bash
    cd ~/  # or your preferred directory
    git clone -b jazzy https://github.com/ROBOTIS-GIT/ai_worker.git
    cd ai_worker
  2. Use the container.sh helper script to manage the container:

    bash
    ./docker/container.sh start
    ./docker/container.sh enter
    ./docker/container.sh stop

Docker Command Guide ​

The container.sh script provides the following commands:

  • help: Display the help message.
  • start: Start the AI Worker container.
  • enter: Enter the running container.
  • stop: Stop the AI Worker container.

Example usage:

bash
./container.sh help
./container.sh start
./container.sh enter
./container.sh stop

Software Update Guide ​

Follow these steps to update the AI Worker or Physical AI Tools packages:

  1. Move to the package directory:

    bash
    cd /path/to/ai_worker_package
    # or
    cd /path/to/physical_ai_tools_package
  2. Switch to the jazzy branch:

    bash
    git checkout jazzy
  3. Pull the latest code:

    bash
    git pull
  4. Restart the container:

    bash
    ./docker/container.sh stop
    ./docker/container.sh start

WARNING

Data stored outside mapped volumes may be lost during container restart. Save important files before restarting the container.

Checking Battery State ​

The FFW-SG2 model has two batteries. The FFW-BG2 model does not use a battery.

To check the battery state, run:

bash
# Check the left battery
ros2 topic echo /ai_worker/battery/left/state --once

# Check the right battery
ros2 topic echo /ai_worker/battery/right/state --once

The output includes the following keys:

  • frame_id: Identifies which battery the message refers to.

    bash
    frame_id: battery_left
  • voltage: Shows the current battery voltage.

    bash
    voltage: 28.700000762939453 # Battery voltage 28.7V
  • percentage: Shows the remaining battery level as a value from 0.0 to 1.0.

    bash
    percentage: 0.934949517250061 # Battery 93% charged

AI Worker and AI Manipulator released under the Apache-2.0 license.