Release Notes
OMX
https://github.com/ROBOTIS-GIT/open_manipulator
4.1.0 (2025-10-24)
- Support OMX-F GUI
- Support OMX-F Keyboard Teleop
- Contributors: Heewon Lee
4.0.10 (2025-10-23)
- Changed default drive mode to 0 for OMX-L
- Contributors: Woojin Wie
4.0.9 (2025-09-15)
- Support custom camera namespace and connection
- Contributors: Junha Cha
4.0.8 (2025-09-03)
- Added camera_usb_cam launch file
- Support OMX series
- Removed unused use_sim_time parameter in the configuration files
- Added OMY-F3M Leader and OMY-L100 Follower configuration files
- Renamed ros2_control files to include operating mode
- Added parameter for enabling spring effect
- Added parameters about scaling factors for input joint velocities and accelerations
- Added usb-cam package dependency in Dockerfile
- Contributors: Woojin Wie, Junha Cha, Wonho Yun
Physical AI Tools
0.6.9 (2025-09-18)
- Changed omx_config.yaml file.
- Contributors: Junha Cha
0.6.8 (2025-08-21)
- Added DatasetInfo.msg, EditDataset.srv, and GetDatasetInfo.srv interfaces for Data Edit communication.
- Added UI features for editing datasets, including merge and delete functionality.
- Added functionality to edit data in the Physical AI Server, including merge and delete operations.
- Added ROS topics and services to receive parameters related to data editing.
- Contributors: Dongyun Kim, Kiwoong Park
0.6.7 (2025-08-18)
- Added a beep sound to signal the start of recording.
- Improved the convenience of data acquisition by using the AI Worker's buttons.
- The right button moves to the next episode, and the left button is for cancellation.
- Contributors: Dongyun Kim
0.6.6 (2025-08-13)
- Fixed an error in the data saving method based on Lerobot.
- Contributors: Dongyun Kim
0.6.5 (2025-08-11)
- Added file browse-related message type
- Added file browser component for policy selection in the inference page
- Added file browsing service with target file checking for policy path selection
- Contributors: Kiwoong Park
0.6.4 (2025-08-07)
- Added training loss display
- Added publishing of current loss during training
- Contributors: Kiwoong Park, Seongwoo Kim
0.6.3 (2025-07-25)
- Fixed a bug to allow setting the output folder path to a specified location.
- Fixed a bug that did not guarantee the order of messages.
- Contributors: Dongyun Kim, Seongwoo Kim, Woojin Wie
0.6.2 (2025-07-24)
- Updated Lerobot to the latest version and modified related functionalities.
- Contributors: Dongyun Kim, Seongwoo Kim, Woojin Wie
0.6.1 (2025-07-23)
- Implemented robust error handling during data collection to prevent server crashes due to incorrect robot type configuration
- Contributors: Seongwoo Kim
0.6.0 (2025-07-23)
- Added training-related service types and message types
- Added a new training page for training imitation learning models
- Implemented a Training Manager to support model training through the Web UI
- Contributors: Kiwoong Park, Seongwoo Kim
0.5.13 (2025-07-21)
- Updated Docker volume mount paths from /root to ${HOME} for improved portability and compatibility
- Contributors: Seongwoo Kim
0.5.12 (2025-07-18)
- Enabled appending video encodings without overwriting existing data in multi-task mode
- Contributors: Seongwoo Kim
0.5.11 (2025-07-16)
- Added functionality for evaluating trained models
- Contributors: Dongyun Kim
0.5.10 (2025-07-15)
- Added multi-tasking data recording support to the Physical AI Server
- Contributors: Kiwoong Park, Seongwoo Kim
0.5.9 (2025-07-07)
- Use global ROS connection instead of multiple instances
- Add proper cleanup for image streams to prevent accumulation
- Remove unnecessary scrollbars in Chrome browser
- Contributors: Kiwoong Park
0.5.8 (2025-07-07)
- Applied Redux Toolkit for better state management
- Added heartbeat status to the UI
- Added heartbeat topic publishing to monitor alive status of Physical AI Server
- Contributors: Kiwoong Park, Dongyun Kim
0.5.7 (2025-06-26)
- Added Image Transport Plugin and fixed missing Gstreamer components
- Contributors: Dongyun Kim
0.5.6 (2025-06-26)
- Reordered pip install order in Dockerfile to fix the numpy version issue
- Contributors: Woojin Wie
0.5.5 (2025-06-26)
- Fixed control panel button states not reflecting correct taskType when switching between Record and Inference pages
- Contributors: Kiwoong Park
0.5.4 (2025-06-25)
- Added support for inference mode in the physical AI Server, including a new InferencePage and related UI components.
- Changed the robot naming format.
- Added Robot Config to support FFW-SG2 robot.
- Added Msg Topic and data acquisition functionality to support Mobile Robot.
- Fixed minor errors in the data acquisition process to improve software stability.
- Added a new inference page for running and monitoring inference tasks.
- Added inference-related msgs and srv types.
- Contributors: Dongyun Kim, Kiwoong Park
0.5.3 (2025-06-16)
- Refactored Physical AI Server for improved data collection capabilities
- Implemented data acquisition functionality using ROS2 topics
- Modified configuration system to allow flexible robot type selection
- Updated data collection method to utilize image buffers for efficiency
- Overall UI improvements for physical_ai_manager
- Added status information display from physical_ai_server
- Added functionality to receive task information from users and send commands to physical_ai_server
- Added bringup launch file that runs physical_ai_server with rosbridge_server and webvideo_server
- Contributors: Dongyun Kim, Kiwoong Park
0.5.2 (2025-05-29)
- Adjusted the waiting timeout for joint states.
- Contributors: Dongyun Kim
0.5.1 (2025-05-29)
- Added quality and transport parameters to image streaming URL
- Added a Docker setup for physical AI server
- Contributors: Kiwoong Park
0.5.0 (2025-05-20)
- Added a web UI for physical AI data collection
- Removed unnecessary dependencies and cleaned up the codebase
- Updated the LeRobot submodule to the latest version
- Refactored to a scalable structure that supports N cameras and various joint configurations
- Contributors: Dongyun Kim, Kiwoong Park, Woojin Wie, Seongwoo Kim
0.4.0 (2025-05-15)
- Added a pipeline for data collection and inference based on ROS2
- Refactored to a scalable structure that supports N cameras and various joint configurations
- Contributors: Dongyun Kim
0.3.1 (2025-05-08)
- Updated the LeRobot submodule to the latest version
- Contributors: Woojin Wie
0.3.0 (2025-04-25)
- Unified multiple launch files into a single configurable launch file for better usability
- Contributors: Seongwoo Kim
0.2.0 (2025-04-08)
- Added a time stamper node for data synchronization purposes
- Removed unused joints and motors bus config
- Contributors: Seongwoo Kim, Hyungyu Kim
0.1.0 (2025-04-07)
- Added a full workflow for recording and visualizing datasets using the LeRobot interface
- Added bringup scripts for system initialization
- Contributors: Seongwoo Kim, Pyo