Skip to content

Model Training ​

This guide walks you through training imitation learning models for OMX, based on datasets collected via the Web UI.

Once preparing your dataset is done, the policy model can be trained using the Web UI.

Model Training ​

1. Prepare Your Dataset ​

The dataset to be used for training should be located at:

USER PC

<your_workspace>/physical_ai_tools/docker/huggingface/lerobot/${HF_USER}/

Datasets collected using Physical AI Tools are automatically saved to that path. However, if you downloaded the dataset from a hub or copied it from another PC, you need to move the dataset to that location.

INFO

  • ${HF_USER} can be any folder name you prefer.
  • <your_workspace> is the directory containing physical_ai_tools

Please refer to the folder structure tree below:

<your_workspace>/physical_ai_tools/docker/.cache/huggingface/lerobot/
  ├── USER_A/           # ← ${HF_USER} folder
  │   ├── dataset_1/    # ← Dataset
  │   │   ├── data/
  │   │   ├── meta/
  │   │   └── videos/
  │   └── dataset_2/
  └── USER_B/
      └── dataset_3/

2. Setup Physical AI Tools Docker Container ​

WARNING

If the Physical AI Tools is already set up, you can skip this step.

If you haven't set up the Physical AI Tools Docker container, please refer to the link below for setup instructions.

Setup Physical AI Tools Docker Container

3. Train the Policy ​

a. Launch Physical AI Server ​

WARNING

If the ai_server is already running, you can skip this step.

Go to physical_ai_tools/docker directory:

USER PC

bash
cd physical_ai_tools/docker

Enter the Physical AI Tools Docker container:

bash
./container.sh enter

Then, launch the Physical AI Server with the following command:

USER PC 🐋 PHYSICAL AI TOOLS

bash
ai_server

b. Open the Web UI ​

Open your web browser and navigate to the Web UI (Physical AI Manager).

(Refer to the Dataset Preparation > Web UI > 1. Open the Web UI for more details.)

On the Home page, select the type of robot you are using.

Web UI

c. Train the Policy ​

Go to the Training page and follow the steps below:

Web UI

At the bottom of the page, select either New Training or Resume Training.

Web UI
Training TypeDescriptionWhen to Use
New TrainingStart training a new model- First time training
- Starting with a new dataset
- Training with a different policy on the same dataset
Resume TrainingContinue training from a saved checkpoint- Training was interrupted and you want to resume
- Want to incorporate additional datasets into the model
- Want to modify training options (Steps, Save Frequency, etc.) and retrain

For new training, follow these steps:

  • Step 1: Select the Dataset, Policy Type and Device.

  • Step 2: Enter the Output Folder Name.

  • Step 3: (Optional) Modify Additional Options if needed.

For more information about these options, please refer to the descriptions below.

  • Training Information

The datasets stored in the ~/.cache/huggingface/ directory on the host (or /root/.cache/huggingface/ inside the Docker container) will be listed automatically. Web UI

Click Start Training to begin training the policy.

Web UI

The training results will be saved in the physical_ai_tools/lerobot/outputs/train/ directory.

(Optional) Uploading Checkpoints to Hugging Face ​

Navigate to physical_ai_tools/docker directory and enter the Docker container:

USER PC

bash
cd physical_ai_tools/docker
bash
./container.sh enter

Navigate to the LeRobot directory:

USER PC 🐋 PHYSICAL AI TOOLS

bash
cd /root/ros2_ws/src/physical_ai_tools/lerobot

To upload the latest trained checkpoint to the Hugging Face Hub:

bash
huggingface-cli upload ${HF_USER}/act_omx_test \
  outputs/train/act_omx_test/checkpoints/last/pretrained_model

This makes your model accessible from anywhere and simplifies deployment.

AI Worker and AI Manipulator released under the Apache-2.0 license.