Skip to content

Manual Packing Procedure for OMY ​

This page describes the procedure for manually moving the OMY to the packing pose when normal operation is unavailable.

Connect OMY with Wizard 2.0 ​

  1. Prepare a PC or laptop with Wizard 2.0 installed.
  2. Connect the Debug USB-C port on the main body panel to the PC using a USB-C cable.
  3. Turn on OMY.
  4. On the PC, check in Device Manager that the Virtual COM port is recognized. connect omy wizard

Search for OMY on Wizard 2.0 ​

  1. In the Wizard 2.0 settings window, select the COM port recognized by the PC. search omy on wizard 1
  2. Click the DYNAMIXEL search button in Wizard 2.0.
  3. Confirm that OMY-HAT (ID 200) is recognized. search omy on wizard 2

Search for DYNAMIXEL-Y on Wizard 2.0 ​

  1. Turn on DXL Power Enable (512) in the OMY-HAT control table. search dynamixelY 1
  2. In Settings -> Search in Wizard 2.0, check the 6 Mbps baud rate and set the ID range to search from 1 to 10. search dynamixelY 2
  3. Click the DYNAMIXEL search button in Wizard 2.0.
  4. Confirm that six DYNAMIXEL-Y actuators (ID 1 to 6) are recognized. search dynamixelY 3

Reset DYNAMIXEL-Y multi-turn alarm ​

  1. Check the ID of the DYNAMIXEL-Y actuator that raised the alarm.
  2. In the Packet Monitoring window of Wizard 2.0, open the COM port and send the Clear command. reset multi-turn alarm
  3. Confirm that the multi-turn alarm has been cleared. reset multi-turn alarm

Manual operation of DYNAMIXEL-Y ​

  1. Change Operating Mode (33) of the target DYNAMIXEL-Y to Current.
  2. Turn the torque on.

WARNING

Caution: The robot may fall in the direction of gravity, so it must be held by hand.

omy manual operation 1 3. Move the target axis to the marked home position. 4. Turn the torque off. 5. Repeat steps 1 to 4 for each axis until the robot reaches the home position or the packing position (see the next block). omy manual operation 2

Initialize the home position ​

  1. Move the robot to the home position.
  2. In the Packet Monitoring window of Wizard 2.0, open the COM port and send the Clear command to IDs 1 through 6. initialize home position 1
  3. Check that the current position of each joint is within 1 degree.
  4. For any joint outside that range, refer to the previous block and manually move it to the home position, then repeat step 2. initialize home position 2

OMY home position ​

Move the robot to the home position by aligning it with the home-position slit. home position slit

OMY packing position ​

  1. Confirm that the robot is in the home position.
  2. Move joint 3 to 150 degrees toward the base panel.
  3. Move joint 4 to 30 degrees. packing position slit

AI Worker and AI Manipulator released under the Apache-2.0 license.