Skip to content

LeRobot Imitation Learning for OMX ​

Overview ​

This tutorial explains how to train a neural network to control OMX autonomously using LeRobot. You'll learn the complete workflow from data collection to model deployment.

By following these steps, you'll be able to replicate tasks such as picking up objects and placing them with high success rates.

Note: This tutorial is based on the Hugging Face LeRobot documentation and adapted specifically for OMX hardware setup.

Before You Begin ​

First, identify the bus servo adapter ports for the leader and follower by running the following command:

bash
lerobot-find-port

You will see an output similar to:

bash
(lerobot) username@username:~/lerobot$ lerobot-find-port
Finding all available ports for the MotorsBus.
Ports before disconnecting: ['/dev/ttyACM1', '/dev/ttyACM0', ...]
Remove the USB cable from your MotorsBus and press Enter when done.

Next, disconnect the USB cable from either the leader or the follower and press Enter to determine the corresponding port. The output will look like this:

bash
The port of this MotorsBus is '/dev/ttyACM1'
Reconnect the USB cable.

For the purposes of this tutorial, we assume:

  • Follower’s port → /dev/ttyACM0
  • Leader’s port → /dev/ttyACM1

Teleoperation ​

You can test if OMX is working properly through teleoperation.

1. Teleoperate OMX ​

Start teleoperation with OMX:

bash
python -m lerobot.teleoperate \
    --robot.type=omx_follower \
    --robot.port=/dev/ttyACM0 \
    --robot.id=omx_follower_arm \
    --teleop.type=omx_leader \
    --teleop.port=/dev/ttyACM1 \
    --teleop.id=omx_leader_arm

Note: the --robot.id/--teleop.id values persist metadata (e.g., calibrations/settings). Use consistent IDs across teleop, recording, and evaluation for the same setup.

2. Teleoperate with Camera ​

For camera integration:

bash
python -m lerobot.teleoperate \
    --robot.type=omx_follower \
    --robot.port=/dev/ttyACM0 \
    --robot.id=omx_follower_arm \
    --robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30}}" \
    --teleop.type=omx_leader \
    --teleop.port=/dev/ttyACM1 \
    --teleop.id=omx_leader_arm \
    --display_data=true

Data Collection ​

1. Record Dataset ​

We use the Hugging Face hub features for uploading your dataset. If you haven’t previously used the Hub, make sure you can log in via the CLI using a write-access token, this token can be generated from the Hugging Face settings.

Add your token to the CLI by running this command:

bash
huggingface-cli login --token ${HUGGINGFACE_TOKEN} --add-to-git-credential

Then store your Hugging Face username in a variable:

bash
HF_USER=$(hf auth whoami | head -n 1)
echo $HF_USER

Record your first dataset:

Note: If you have teleoperation running from the previous step, please stop it first before running this command as it includes teleoperation with camera.

bash
lerobot-record \
    --robot.type=omx_follower \
    --robot.port=/dev/ttyACM0 \
    --robot.id=omx_follower_arm \
    --robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30}}" \
    --teleop.type=omx_leader \
    --teleop.port=/dev/ttyACM1 \
    --teleop.id=omx_leader_arm \
    --display_data=true \
    --dataset.repo_id=${HF_USER}/record-test \
    --dataset.num_episodes=5 \
    --dataset.single_task="Pick up the Dynamixel Motor"

2. Recording Controls & Details ​

Keyboard Shortcuts:

  • Right Arrow (→): End episode and move to next
  • Left Arrow (←): Cancel episode and re-record
  • Escape (ESC): Stop session and upload dataset

Recording Parameters:

bash
--dataset.episode_time_s=60    # Episode duration (default: 60s)
--dataset.reset_time_s=60      # Reset time (default: 60s)
--dataset.num_episodes=50      # Total episodes (default: 50)

Additional behavior:

  • Disable automatic push to the Hub with --dataset.push_to_hub=false (default: true)
  • Resume a failed/interrupted session with --resume=true
    • When resuming, set --dataset.num_episodes to the number of additional episodes to record (not the final total)

3. Dataset Management ​

Local Storage:

  • Dataset stored in: ~/.cache/huggingface/lerobot/{repo-id}

Dataset Upload:

bash
huggingface-cli upload ${HF_USER}/record-test ~/.cache/huggingface/lerobot/${HF_USER}/record-test --repo-type dataset
echo https://huggingface.co/datasets/${HF_USER}/record-test

Data Visualization ​

View Dataset Online ​

If uploaded to the Hub (either by default behavior or with --dataset.push_to_hub=true), you can visualize your dataset online by copy pasting your repo id given by:

bash
echo ${HF_USER}/record-test

Replay Episodes ​

Replay recorded episodes:

bash
lerobot-replay \
  --robot.type=omx_follower \
  --robot.port=/dev/ttyACM0 \
  --robot.id=omx_follower_arm \
  --dataset.repo_id=${HF_USER}/record-test \
  --dataset.episode=0 # choose the episode you want to replay

Model Training ​

1. Train Policy ​

Train your imitation learning model:

bash
lerobot-train \
  --dataset.repo_id=${HF_USER}/record-test \
  --policy.type=act \
  --output_dir=outputs/train/omx_act_policy \
  --job_name=act_record-test \
  --policy.device=cuda \
  --wandb.enable=true \
  --policy.repo_id=${HF_USER}/omx_act_policy

Let’s break down the command:

  • Dataset repo: We point --dataset.repo_id to your training dataset. In this guide it’s ${HF_USER}/record-test.

  • Policy type: --policy.type=act selects the ACT policy. It loads the appropriate configuration and automatically adapts to your robot’s setup (motor state/action dimensions and any cameras) as stored in the dataset.

  • Compute device: --policy.device=cuda runs on an NVIDIA GPU. On Apple Silicon, use --policy.device=mps.

  • Experiment logging (optional): --wandb.enable=true enables Weights & Biases logging. If you use it, make sure you’re logged in first:

    bash
    wandb login

TIP

If you do not want to push your trained model to the Hugging Face Hub, use the option --policy.push_to_hub=false instead of --policy.repo_id=${HF_USER}/omx_act_policy.

2. Resume Training ​

To resume training from the latest checkpoint:

bash
python -m lerobot.scripts.train \
  --config_path=outputs/train/omx_act_policy/checkpoints/last/pretrained_model/train_config.json \
  --resume=true

3. Upload Checkpoints (Optional) ​

To upload your trained model to the Hugging Face Hub:

bash
huggingface-cli upload ${HF_USER}/omx_policy \
  outputs/train/omx_act_policy/checkpoints/last/pretrained_model

Model Evaluation ​

Run inference and evaluate your policy ​

Evaluate your trained model:

bash
python -m lerobot.record \
  --robot.type=omx_follower \
  --robot.port=/dev/ttyACM0 \
  --robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 1920, height: 1080, fps: 30}}" \
  --robot.id=omx_follower_arm \
  --display_data=false \
  --dataset.repo_id=${HF_USER}/eval_act_omx \
  --dataset.single_task="Pick and place object" \
  --policy.path=${HF_USER}/omx_act_policy

Note: use an eval_* dataset name (e.g., eval_act_omx) to clearly separate evaluation runs.

As you can see, it’s almost the same command as previously used to record your training dataset. Two things have changed:

  • There is an additional --policy.path argument which indicates the path to your policy checkpoint (e.g., outputs/train/eval_act_omx/checkpoints/last/pretrained_model). You can also use the model repository if you uploaded a model checkpoint to the hub (e.g., ${HF_USER}/omx_act_policy).
  • The dataset name begins with eval_ to reflect that you are running inference (e.g., ${HF_USER}/eval_act_omx).

AI Worker and AI Manipulator released under the Apache-2.0 license.