Model Inference with LeRobot CLI
Once your model is trained, you can deploy it on the OMY for inference.
Model Deployment and Inference
1. Transfer Model to Robot PC
INFO
If you trained your model directly on NVIDIA Jetson AGX Orin, you can skip this step.
Change ownership of the model directory. This step must be performed on the robot PC, not inside the Docker container:
sudo chown -R robotis ./
Move your model folder from your local PC to the model directory on the Robot PC using scp
:
scp -r <your model folder's directory> robotis@<your robot's serial number>.local:~/open_manipulator/docker/lerobot/outputs/train
2. Open a Terminal and Enter the Docker container
cd open_manipulator && ./docker/container.sh enter
3. Launch the ROS 2 Follower Node
ros2 launch open_manipulator_bringup omy_f3m.launch.py
4. Run Inference
a. Open a New Terminal and Run Docker Container
Open a terminal on the Jetson device and enter the Docker container:
cd open_manipulator && ./docker/container.sh enter
b. Navigate to the LeRobot
Directory
cd /root/ros2_ws/src/physical_ai_tools/lerobot
c. Run the Following Command for Evaluation
python lerobot/scripts/control_robot.py \
--robot.type=omy \
--control.type=record \
--control.single_task="pick and place objects" \
--control.fps=15 \
--control.repo_id=${HF_USER}/eval_omy_test \
--control.tags='["tutorial"]' \
--control.episode_time_s=20 \
--control.reset_time_s=10 \
--control.num_episodes=10 \
--control.push_to_hub=true \
--control.policy.path=outputs/train/act_omy_test/checkpoints/last/pretrained_model \
--control.play_sounds=false
👉 Key Inference Parameters
Parameter | Description |
---|---|
--control.type=record | Records the policy performance for later evaluation |
--control.policy.path | Path to your trained model checkpoint |
--control.episode_time_s | Duration of each inference episode (in seconds) |
--control.repo_id | Hugging Face repo where evaluation results will be saved |
Visualizing Inference Results
After running inference, you can visualize the results using the same visualization tool used for datasets:
python lerobot/scripts/visualize_dataset_html.py \
--host 0.0.0.0 \
--port 9091 \
--repo-id ${HF_USER}/eval_omy_test
Then open http://127.0.0.1:9091 in your browser to see how your model performed.
TIP
If you have another device connected to the same network as the host machine, open http://{robot type}-{serial number}.local:9091
in your browser to see how your model performed.
For example, http://omy-SNPR48A0000.local:9091
.
Troubleshooting
- Out of memory errors: Try reducing the batch size with
--train.batch_size=16
or lower - Low performance: Consider collecting more diverse training data or increasing training duration
- Robot not responding: Ensure the follower node is running and communication is established
- Training divergence: Check your dataset quality and try decreasing the learning rate