Skip to content

Dataset Preparation with Web UI

Prerequisites

This section describes the necessary setup steps before starting data preparation. To begin data preparation, access the Robot PC either directly or via SSH. See the Setup Guide for instructions on how to connect via SSH.

1. Launch the ROS 2 teleoperation node

a. Open a terminal and enter the Docker container:

cd ai_worker && ./docker/container.sh enter

b. Then, launch the ROS 2 teleoperation node using the appropriate command for your robot type:

ffw_bg2_ai

2. Launch Physical AI Server

INFO

The Physical AI Server is the backend that connects with the Web UI. It should be running to use the interface for data recording.

Open a terminal and enter the Docker container:

cd ai_worker && ./docker/container.sh enter

Launch Physical AI Server with the following command:

bash
ros2 launch physical_ai_server physical_ai_server_bringup.launch.py

Or, use shortcut command:

bash
ai_server

3. Open the Web UI

INFO

This step must be performed on the host machine (or another device on the same network).

Identify the serial number of the AI Worker device. In this example, the serial number is SNPR48A0000.

Access the Web UI in Your Browser

Open your web browser and go to http://{robot type}-{serial number}.local, replacing {serial number} with the serial number from the previous step.

For example:

  • http://ffw-SNPR48A0000.local

Once connected, you should see the web UI as shown below.

Web UI

Record your dataset

1. Select the Robot Type

On the Home page, select the type of robot you are using.

Web UI

2. Go to Record page

INFO

You cannot access Record page unless a robot type has been selected on the Home page. Please ensure that the robot type is selected before proceeding.

The Record page is divided into three main sections:

  • Image Streaming Area (Center): Displays real-time camera streams from the robot.

  • Task Info Panel (Right side): Enter task name, task instruction, time values, etc. (details)

  • Control Panel (Bottom): Start/stop recording and manage data collection. (details)

The selected robot type is also displayed in the top left corner.

Web UI

3. Visualize RGB images from the cameras:

The image stream is displayed automatically upon entering the Record page. You can remove the current stream and select a different one as needed.

To change the image topic:

  1. Click the + button in the Image Streaming Area.
  2. Choose a topic from the popup window.
Web UI

4. Enter Task Information:

Fill out the task-related fields in the Task Info Panel, located on the right side of the Record page.

Web UI

For detailed information on each field, expand the section below:

👉 Task Information Field Descriptions
ItemDescription
Task NameIt is used for the folder name of the dataset
Task InstructionIt is a sentence that instructs the robot what action to perform, such as "pick and place object"
Push to hubIf you want to push the dataset to the Hugging Face Hub, check this box. This allows sharing and training.
To push to the Hugging Face Hub, you need to:
1. Have a Hugging Face account
2. Have the necessary permissions to push to the repository
Private ModeOnly available when "Push to hub" is checked. Keeps your dataset private on Hugging Face.
User IDYour Hugging Face account username, also used as the folder name for the dataset.
- If not using Hugging Face, you can use any name.
- If using Hugging Face, click "Load" to select from registered User IDs.
- If no User IDs or want a different one, click "Change" and enter your Hugging Face token.
- If you have a registered account but haven't checked "Push to hub", you can either:
1. Load a registered User ID
2. Manually enter any User ID
FPSFrame rate for dataset recording. Recommended value is 15.
TagsKeywords to categorize and organize your dataset in the hub. Multiple tags can be added. Useful for searching or filtering later.
Warmup TimeDuration (in seconds) to warm up the robot before starting the recording
Episode TimeDuration (in seconds) to record each episode
Reset TimeTime allocated (in seconds) for resetting between episodes
Num EpisodesTotal number of episodes to record
Optimized SaveIf enabled, uses RAM for faster dataset encoding processing

5. Start Recording:

To begin recording, use the Control Panel located at the bottom of the Record page:

Web UI

Step 1: Click the Start Button

Click the Start button to begin the recording session. The system will automatically:

  • Warm up the robot for the specified Warm-up Time
  • Record each episode for the specified Episode Time
  • Wait for the specified Reset Time between episodes
  • Repeat the above steps for the specified Number of Episodes

Step 2: Monitor and Control During Recording

While recording is in progress, the following controls are available:

  • The Stop button saves the current episode in progress and stops the recording. If you press the Start button again, recording will resume from the next episode.
  • The Retry button cancels the current episode and restarts recording for that episode
  • The Next button ends the current episode early and moves to the next episode
  • The Finish button ends the recording session and saves the current dataset, regardless of the remaining number of episodes

INFO

  • The current recording stage is displayed in the control panel:

    • 📍 Ready to start — Standby mode before recording begins
    • 🔥 Warm-up in progress — Robot is warming up
    • 🔴 Recording in progress — Capturing data
    • 🏠 Reset in progress — Reset time between episodes
    • 💾 Saving... — Encoding and saving the episode

TIP

  • Before you start, keep the robot in a safe and ready position during warm-up
  • Make sure all required fields in the Task Info Panel are filled in
  • Keep the robot in a safe and ready position during warm-up
  • Monitor progress and status updates through the Web UI
  • System resources (CPU, RAM, Storage) are displayed during recording

Step 3. After recording:

  • The dataset will be saved locally.
  • If "Push to hub" is enabled, the dataset will be uploaded to Hugging Face.
  • You can find the recorded dataset in the location below:

INFO

This path refers to the host system, not inside the Docker container.

~/ai_worker/docker/huggingface/lerobot

Dataset Visualization

Once data collection is complete, you can preview and inspect your recorded dataset using the following command:

bash
cd /root/ros2_ws/src/physical_ai_tools/lerobot
bash
python lerobot/scripts/visualize_dataset_html.py \
  --host 0.0.0.0 \
  --port 9091 \
  --repo-id ${HF_USER}/ffw_test

You should see an output similar to the following:

Fetching 4 files: 100%|██████████| 4/4 [00:00<00:00, 3457.79it/s]
.gitattributes: 100%|██████████| 2.46k/2.46k [00:00<00:00, 45.9MB/s]
Fetching 126 files: 100%|██████████| 126/126 [00:00<00:00, 266.66it/s]
Resolving data files: 100%|██████████| 30/30 [00:00<00:00, 662258.53it/s]
INFO 2025-05-15 16:18:07 set_html.py:364 Output directory already exists. Loading from it: '/tmp/lerobot_visualize_dataset_uo6ddbb1'
 * Serving Flask app 'visualize_dataset_html'
 * Debug mode: off
INFO 2025-05-15 16:18:07 _internal.py:97 WARNING: This is a development server. Do not use it in a production deployment. Use a production WSGI server instead.
 * Running on http://127.0.0.1:9091
INFO 2025-05-15 16:18:07 _internal.py:97 Press CTRL+C to quit

Access http://127.0.0.1:9091 to view the dataset. You should see a web interface similar to the one below: Web UI

TIP

Once the server is running, open http://127.0.0.1:9091 in your browser to preview the dataset.

TIP

On a device connected to the same network as the host machine, open http://ffw-{serial number}.local:9091 in your browser to preview the dataset.

For example, http://ffw-SNPR48A0000.local:9091.

AI Worker and AI Manipulator released under the Apache-2.0 license.